Zap mosquitos in my bedroom using a crazyflie carrying a laser

I probably dont have the experience to create such a system. However the idea is open to anyone who feels like picking it up and running with it. Here are my thoughts so far. Sometimes I am lying in bed and hear the awful sound of a marauding mosquito looking to bite me. I think only female mosquitos are equipped for the biting task. It might be possible to home in on the high frequency sound produced by the mosquito. Three sensors in the room might provide accurate position of insect and transmit it to crazyflie. If the crazyflie can carry a laser then it might use the position information to zap the insect. Any ideas welcome