“XIAO” schematic & footprint Library is available?
I want to use on “KIcad”.
on Github is OLD ver than Release Product.
thanks a lot @ansonhe97!
I update under pad 4dot and Vin/GND.
But position is not precise (measure by vernier caliper)
Colud you fix that?
Updated to wiki, check the resources again, and it should be it!
@ansonhe97 Is there Altium Designer library available?
Did you ever find one? I couldn’t so I have been working on some for our internal library. But I found that the pads in the DXF file on the wiki do not align properly with the pads in the STP file on the wiki, and I have not idea which is correct.
I totally forgot I had registration here. Anyway, I have an Integrated Library(IntLib) somewhere. I will upload it first thing tomorrow at noon. In the meantime check SnapEDA Search, 95% sure you will find for every variant of the XIAO or use the Altium import wizard. If you need help with the pcb or Altium fell free to contact me.