Hi all.
I’m using the XIAO RA4M1 with the Arduino IDE.
I noticed that the startup time from power on to executing a command in the Arduino setup procedure is approximately 500 ms.
I tested this with a program that only sets one output in the setup procedure.
Channel 0 shows the PowerOn and channel 1 the output-pin
I think the reason is the bootloader.
Does anybody have a idea how I can activate the bootloader only when powering on AND pressing the B button, so that the startup time is reduced to a minimum when powering on ?
BR Juergen