WiFi 连接成功! IP 地址: 10.161.162.192 PSRAM已启用,总大小: 8385911 字节 可用PSRAM: 8371247 字节 E (3770) camera: Camera probe failed with error 0x105(ESP_ERR_NOT_FOUND) E (3770) gdma: gdma_disconnect(299): no peripheral is connected to the channel 摄像头初始化失败: 0x105
=== 系统就绪 === WiFi IP: 10.161.162.192 照片上传: http://8.140.192.226:8000/img_get/ 拍照间隔: 1秒
我尝试换过XIAOesp32s3sense,会出现第一次拍照成功,然后,后面全部失败的情况
·
hi there what bsp file version , roll back to older one. in boards tab select exp32 and pulldown to older release , look at other threads too,
HTH GL PJ