XIAO nRF54L15 and Wio-SX1262 doesn't work on Zephyr

Hi guys, I’m trying to use a Wio-SX1262 module with a XIAO nRF54L15 and Zephyr, but it just doesn’t work. I tested with an Arduino example, and it works (Some guy did a port to Arduino but looks like something’s doesn’t work, like the NVS storage didn’t was implemented because I can’t Join correctly, but I can see that the intent on my Gateway)

For all I say before I know is not a wiring problem, it’s something with Zephyr.

My app.overlay is this

/ {
	/*
	  * @brief Device Tree Overlay for XIAO nRF54L15
	  *
	  * This file customizes the base board device tree to configure
	  * peripherals for a specific application, including:
	  * - SX1262 via SPI
	  */

	//Aliases for easy access to devices in application code
	aliases {
		lora0 = &lora0;
		spi0 = &xiao_spi;
	};
};

// SPI peripheral
&xiao_spi {
	compatible = "nordic,nrf-spim";
	status = "okay";
	// D0 pin for Chip Select
	cs-gpios = <&xiao_d 0 GPIO_ACTIVE_LOW>;

	//Lora module
	lora0: sx1262@0 {
		compatible = "semtech,sx1262";
		reg = <0>;
		label = "SX1262";

		spi-max-frequency = <8000000>;

		reset-gpios = <&xiao_d 2 GPIO_ACTIVE_LOW>;
		//antenna-enable-gpios = <&xiao_d 4 GPIO_ACTIVE_LOW>;
		busy-gpios = <&xiao_d 3 GPIO_ACTIVE_HIGH>;
		dio1-gpios = <&xiao_d 1 GPIO_ACTIVE_HIGH>;
		//rx-enable-gpios = <&xiao_d 4 GPIO_ACTIVE_HIGH>;
	};
};

My prj.conf is this

CONFIG_GPIO=y
CONFIG_SPI=y
CONFIG_LORA=y
CONFIG_LORA_SX126X=y
CONFIG_LORAWAN=y
CONFIG_LORAWAN_REGION_EU868=y
CONFIG_MAIN_STACK_SIZE=2048
CONFIG_SYSTEM_WORKQUEUE_STACK_SIZE=2048
CONFIG_LOG=y
CONFIG_LOG_DEFAULT_LEVEL=3
CONFIG_LORAWAN_LOG_LEVEL_DBG=y
CONFIG_PRINTK=y
CONFIG_DEBUG=y
CONFIG_DEBUG_OPTIMIZATIONS=y

I always get this output:

*** Booting Zephyr OS build v4.4.0-rc1 ***
[00:13:45.893,905] <dbg> lorawan: lorawan_set_region: Selected region 5
[00:13:45.939,396] <dbg> lorawan: lorawan_start: LoRaMAC Initialized
[00:13:45.939,409] <inf> lorawan_class_a: Joining network over OTAA

And nothing more happend!

I’m using this example: zephyr/samples/subsys/lorawan/class_a at main · zephyrproject-rtos/zephyr · GitHub

Thanks for you help

Hi there,

SO I wouldn’t be so Quick with that…:grin:
Your overlay is not obviously wrong, but it is probably incomplete for the SX1262. The most likely problem is not Zephyr in general — it is that the SX1262 driver needs the board control lines defined exactly right, especially DIO1, BUSY, RESET, and often RF-switch control (tx-enable-gpios, rx-enable-gpios, or dio2-tx-enable). Zephyr supports all of those, but your current overlay only defines part of the radio interface.

Try this and the other tweaks see if you don’t get it or closer…

/ {
	aliases {
		lora0 = &lora0;
	};
};

&xiao_spi {
	status = "okay";
	cs-gpios = <&xiao_d 0 GPIO_ACTIVE_LOW>;

	lora0: sx1262@0 {
		compatible = "semtech,sx1262";
		reg = <0>;
		spi-max-frequency = <1000000>;

		reset-gpios = <&xiao_d 2 GPIO_ACTIVE_LOW>;
		busy-gpios  = <&xiao_d 3 GPIO_ACTIVE_HIGH>;
		dio1-gpios  = <&xiao_d 1 GPIO_ACTIVE_HIGH>;

		/* Use these only if the board really has separate RF switch control */
		/* tx-enable-gpios = <&xiao_d 4 GPIO_ACTIVE_HIGH>; */
		/* rx-enable-gpios = <&xiao_d 5 GPIO_ACTIVE_HIGH>; */

		/* Or, if the module uses DIO2 to control RF switching: */
		/* dio2-tx-enable; */

		status = "okay";
	};
};

I do not think You have enough evidence to say “Zephyr is broken.”

I think it is more likely one of these:

  • wrong GPIO mapping
  • missing RF switch control
  • wrong GPIO polarity
  • SPI bus/pinctrl not actually resolving how he thinks on the nRF54L15 board

That is the old story with radios:
Arduino can limp through a partial setup; Zephyr usually makes you get the hardware description right.

Try this,

  • Open build/zephyr/zephyr.dts and confirm &xiao_spi and &xiao_d resolve the way you think.
  • Lower SPI first to 1000000 or even 500000 until the radio is proven alive.
  • Confirm the exact Wio-SX1262 control lines:

:face_with_monocle:

HTH
GL :slight_smile: PJ :v:

@xyz15

Has there been an update? I am having an issue with the nrf52840 and the Wio-SX1262. The lora module initializes fine but does not tx or rx anything. What are the correct dts configs to use?

this work with me using nRF Connect SDK v3.2.4 and Seeed Studio XIAO nRF54L15 (non-Sense variant) \+ Wio-SX1262 LoRa Kit

#include <dt-bindings/lora/sx126x.h>
#include <zephyr/dt-bindings/adc/adc.h>

/* SX1262 on spi00 (P2.01=SCK, P2.02=MOSI, P2.04=MISO) */
&spi00 {
status = “okay”;
cs-gpios = <&gpio1 10 GPIO_ACTIVE_LOW>;

lora0: sx1262@0 {
	compatible = "semtech,sx1262";
	reg = <0>;
	spi-max-frequency = <DT_FREQ_M(8)>;
	reset-gpios              = <&gpio1 6 GPIO_ACTIVE_LOW>;
	busy-gpios               = <&gpio1 7 GPIO_ACTIVE_HIGH>;
	dio1-gpios               = <&gpio1 5 GPIO_ACTIVE_HIGH>;
	dio2-tx-enable;
	dio3-tcxo-voltage        = <SX126X_DIO3_TCXO_1V8>;
	tcxo-power-startup-delay-ms = <5>;
};

};