Hi M-Rafay_Shams,
I’m using this sketch successfully with a TTL level device connected to the TX & RX pins on the Expansion board. You may be able to use this a starting point It basically starts and looks for a “<” to begin , sending a “N” or a “D” command to the device and it responds with the strings listed, I parsed them for what I needed, “Serial1” is the port for those pins on the Xiao 6 & 7. I have some pictures of the connections on here in other posts.
//----------------------------------------------------------------------------------------------
//Get DUT data
//Board Library : Seeed nRF52 mbed-enable Borads 2.9.1
//Board Select : Seeed nRF52 mbed-enable Borads / Seeed XIAO BLE - (nRF52840)
//<
//N
// NS8135-0201ORafael Farinas LPN135M135UMT92 B8.02
//D
//
//D0305040T1879t 16+5Z0000H0042278N0037055F9999999V010.5E+073z0000S8135-0201
//
//
//----------------------------------------------------------------------------------------------
#include <Arduino.h>
#include <U8x8lib.h>
#define LED LEDG
//Create a instance of class
U8X8_SSD1306_128X64_NONAME_HW_I2C u8x8(/* clock=*/PIN_WIRE_SCL, /* data=*/PIN_WIRE_SDA, /* reset=*/U8X8_PIN_NONE); // OLEDs without Reset of the Display
const byte numChars = 32;
char receivedChars[numChars];
boolean newData = false;
int ndx = 0;
//boolean lelsPower = false;
int lelsReady = 0;
//char string = [20];
void setup() {
Serial1.begin(9600);
Serial.begin(9600);
while (!Serial);
delay(3000);//relax...Get Ready for serial port
Serial.println();
Serial.println("Power ON \n "); // Let's BEGIN!!
Serial.println("Test program" __FILE__ " compiled on " __DATE__ " at " __TIME__);
Serial.println();
Serial.println("Processor came out of reset.");
//Serial1.println();
u8x8.begin();
u8x8.setFlipMode(1); // set number from 1 to 3, the screen word will rotary 180
u8x8.setFont(u8x8_font_8x13B_1x2_r);
u8x8.clearDisplay();
u8x8.setCursor(0, 0);
u8x8.print("Power ON ");
//delay(3000);
Serial.println("Serial initialized.");
Serial.println("Serial1 initialized.");
// Wait for lels to power on
delay(200);
checkLelsStartup();
//lelsPower();
}
void loop() {
if (!lelsReady) {
Serial.println("DUT is powered OFF");
// wait for user input
Serial.println("Press any key to continue...");
while (!Serial.available()) {
// do nothing
}
// read and discard the user input
Serial.read();
//lelsPower();
} else {
Serial.println("DUT is Powered ON!.");
// Send "N" command to lels
Serial1.write(0x4E); // Send hex 4E command
Serial1.write(0x0D); // Send hex 0D command
delay(150); // Wait for response
u8x8.print("LeL ON ");
// Check for response
String response = "";
while (Serial1.available()) {
char c = Serial1.read();
response += c;
if (c == 0x0D) { // Check for carriage return
delay(10); // Wait for line feed
response += Serial1.read(); // Read line feed character
break;
}
}
Serial.print("LeLs Fixed Data:"); // Print response to serial monitor
// Split response into tags
String tags[9] = {"S", "O", "L", "N", "M", "U", "T"," ","B"};
int tagIndex = 0;
for (int i = 0; i < response.length(); i++) {
if (response.charAt(i) == tags[tagIndex].charAt(0)) {
Serial.print(tags[tagIndex] + ": ");
tagIndex++;
}
Serial.print(response.charAt(i));
if (tagIndex >= 10) {
break;
}
if (response.charAt(i) == ' ') {
Serial.print("\t");
}
}
Serial.println();
response.trim();
printTags1(response);
// Wait for 20 seconds before sending "D" command
delay(1000);
sendThed();
Serial.print("LeLs Variable Data:"); // Print response to serial monitor
// Split response into tags
String varTags[14] = {"D", "T", "z", "t", "F", "N", "M", "S", "V", "E", "H", "U", "Z", "O"};
tagIndex = 0;
for (int i = 0; i < response.length(); i++) {
if (response.charAt(i) == varTags[tagIndex].charAt(0)) {
Serial.print(varTags[tagIndex] + ": ");
tagIndex++;
}
Serial.print(response.charAt(i));
if (tagIndex >= 14) {
break;
}
if (response.charAt(i) == ' ');
}
response.trim();
printTags(response);
}
delay(30000);
}
//========================functions===============
String printTags(String response) {
// Extract the relevant fields from the response
String s = response.substring(1, 10);
String o = response.substring(10, 41);
String l = response.substring(41, 42);
String n = response.substring(42, 45);
String m = response.substring(45, 48);
String u = response.substring(48, 49);
String t = response.substring(49, 51);
String b = response.substring(54, 56);
// Construct the formatted string
String data2 = "Pre-Defined Set of Calculated Data \n";
data2 += " S:" + s + "\n";
data2 += " O:" + o + "\n";
data2 += " L:" + l + "\n";
data2 += " N:" + n + "\n";
data2 += " M:" + m + "\n";
data2 += " U:" + u + "\n";
data2 += " T:" + t + "\n";
data2 += " B:" + b + "\n";
return data2;
}
void sendThed(){ // Send "D" command to lels
Serial1.write(0x44); // Send hex 44 command
Serial1.write(0x0D); // Send hex 0D command
delay(150); // Wait for response
// Check for response
String response = "";
while (Serial1.available()) {
char c = Serial1.read();
response += c;
if (c == 0x0D) { // Check for carriage return
delay(10); // Wait for line feed
response += Serial1.read(); // Read line feed character
break;
}
}
Serial.println(response); // Print response to serial monitor
String data2 = printTags(response); // two response strings
Serial.println(data2); // Print formatted data to serial monitor
}
bool checkLelsStartup() {
Serial.println("Checking Lels Communication");
while (Serial1.available()) {
char c = Serial1.read();
if (c == '<') {
delay(10);
char next1 = Serial1.read();
char next2 = Serial1.read();
if (next1 == 0x0A && next2 == 0x0D) {
Serial.println("recieved power up");
lelsReady = 1;
return true;
}
}
}
/*
// If we didn't find the powerup string, wait for baud rate change and try again
Serial.println("Checking Lels Communication Low Speed");
Serial1.write("\r");
delay(10);
Serial.println("sending l/f ");
while (Serial1.available()) {
char c = Serial1.read();
if (c == '<') {
delay(10);
char next1 = Serial1.read();
char next2 = Serial1.read();
if (next1 == 0x0A && next2 == 0x0D) {
return true;
}
}
}
*/
Serial.println("didn't find the powerup string");
lelsReady = 0;
return false;
}
bool lelsPower() {
Serial.println("Checking Lels Power");
String response = "";
while (Serial1.available()) {
char c = Serial1.read();
if (c == '<') {
response += c;
delay(10);
if (Serial1.read() == 0x0A) {
delay(10);
if (Serial1.read() == 0x0D) {
}
Serial.println("Lels READY!!");
int lelsReady = 1;
}return true;
}
}
lelsReady = 0;
Serial.println(" Lels is NOT powered " );
return false;
//Serial.println(response);
}
void printTags1(String data) {
String tags[9] = {"S", "O", "L", "N", "M", "U", "T", " ","B"};
int tagLengths[9] = {11, 31, 1, 3, 3, 1, 2, 2, 3};
int dataIndex = 0;
Serial.println("TAG\t\tVALUE");
Serial.println("------------------------");
for (int i = 0; i < 9; i++) {
String tagValue = data.substring(dataIndex, dataIndex + tagLengths[i]);
dataIndex += tagLengths[i];
Serial.println(tags[i] + ":\t" + tagValue);
}
}
void printTags2(String data) {
String tags[11] = {"S", "O", "L", "N", "M", "U", "T", "B", "X", "Y", "Z"};
int tagLengths[11] = {9, 31, 1, 3, 3, 1, 2, 2, 4, 4, 4};
int dataIndex = 0;
Serial.println("TAG\t\tVALUE");
Serial.println("------------------------");
for (int i = 0; i < 11; i++) {
String tagValue = data.substring(dataIndex, dataIndex + tagLengths[i]);
dataIndex += tagLengths[i];
Serial.println(tags[i] + ":\t" + tagValue);
}
}
void initdisplay() {
pinMode(LEDR, OUTPUT); // initialize the LED pin as an output:
pinMode(LEDG, OUTPUT); // initialize the LED pin as an output:
pinMode(LEDB, OUTPUT);
pinMode(LED_BUILTIN, OUTPUT); // initialize the LED pin as an output:
u8x8.begin();
u8x8.setFlipMode(1); // set number from 1 to 3, the screen word will rotary 180
u8x8.setFont(u8x8_font_8x13B_1x2_r);
u8x8.clearDisplay();
u8x8.setCursor(0, 0);
u8x8.print("Power ON ");
}
void setupblink() {
setLedRGB(false, true, false); // Red
delay(1000);
setLedRGB(true, false, false); // Green
delay(1000);
setLedRGB(false, false, true); // Blue
delay(1000);
setLedRGB(false, false, false); // OFF
}
void setLedRGB(bool red, bool green, bool blue) {
if (!blue) {
digitalWrite(LEDB, HIGH);
} else {
digitalWrite(LEDB, LOW);
}
if (!green) {
digitalWrite(LEDG, HIGH);
} else {
digitalWrite(LEDG, LOW);
}
if (!red) {
digitalWrite(LEDR, HIGH);
} else {
digitalWrite(LEDR, LOW);
}
}
As far as SDK and NRF connect Install the tool chain and click the “First Step” it will walk you through building app and code with Zephyr.
HTH
GL 
PJ