XIAO NRF52840 - Bluetooth connection disconnects after sending "on" signal

I’ve got a working Bluetooth connection to act as a remote switch. Which works on its own but once I add in the addition IMU and PID control code the Bluetooth connections disconnects right as I send my on signal. There are three PID loops running in my code and if I removed one of them the code runs just fine but its no specific loop. I’ve tried commenting out each loop while having all other remaining and it seems to be the number of loops and not which ones are running.

#include <PID_v1.h>
#include <ArduinoBLE.h>
#include "LSM6DS3.h"
#include "Wire.h"

BLEService onSwitch("19B10000-E8F2-537E-4F6C-D104768A1214");  //Bluetooth Low Energy Switch Service

//Bluetooth Low Energy Switch Characteristic - custom 128-bit UUID, read and writable by central
BLEByteCharacteristic switchCharacteristic("19B10001-E8F2-537E-4F6C-D104768A1214", BLERead | BLEWrite);

//Create a instance of class LSM6DS3
LSM6DS3 myIMU(I2C_MODE, 0x6A);  //I2C device address 0x6A

double InputX, OutputX, InputY, OutputY, Setpoint, InputZ, OutputZ, PWMZ;
int CLKWiseX = 0;  //Motors for tilt control about the X axis
int AntiCLKWiseX = 2;
int CLKWiseY = 4;  //Motors for tilt control about the Y axis
int AntiCLKWiseY = 6;
int ZAxis = 9;  //Motor for rotation control about the Z axis

//PID parameters, for X and Y axis control these parameters are assumed to be equivalent
double kp = 0.5;
double ki = 1;
double kd = 0.01;
double kpZ = 0.5;
double kiZ = 1;
double kdZ = 0.01;

bool On = false;

PID myPIDX(&InputX, &OutputX, &Setpoint, kp, ki, kd, DIRECT);     //Initialize PID, X axis
PID myPIDY(&InputY, &OutputY, &Setpoint, kp, ki, kd, DIRECT);     //Initialize PID, Y axis
PID myPIDZ(&InputZ, &OutputZ, &Setpoint, kpZ, kiZ, kdZ, DIRECT);  //Initialize PID, Z axis

void setup() {
  // put your setup code here, to run once:
  Serial.begin(9600);
  //Initialize bluetooth and IMU communication.
  myIMU.begin();
  BLE.begin();
  BLE.setLocalName("Micro");
  BLE.setAdvertisedService(onSwitch);
  onSwitch.addCharacteristic(switchCharacteristic);
  BLE.addService(onSwitch);
  switchCharacteristic.writeValue(0);
  BLE.advertise();

  //Set PID to automatic and define output limits to allow for negative rotation
  myPIDX.SetMode(AUTOMATIC);
  myPIDX.SetOutputLimits(-255, 255);
  myPIDY.SetMode(AUTOMATIC);
  myPIDY.SetOutputLimits(-255, 255);
  myPIDZ.SetMode(AUTOMATIC);
  myPIDZ.SetOutputLimits(-127, 127);
  Setpoint = 0;

  pinMode(CLKWiseX, OUTPUT);
  pinMode(AntiCLKWiseX, OUTPUT);
  pinMode(CLKWiseY, OUTPUT);
  pinMode(AntiCLKWiseY, OUTPUT);
  pinMode(ZAxis, OUTPUT);

  //analogWrite(ZAxis, 127);  //The motor for Z axis control is set to be a momentum wheel all others are reaction wheels
}

void loop() {
  // put your main code here, to run repeatedly:
  //Listen for Bluetooth Low Energy peripherals to connect:
  BLEDevice central = BLE.central();

  //While the central is still connected to peripheral:
  if (central.connected()) {
    if (switchCharacteristic.written()) {
      if (switchCharacteristic.value()) {
        On = false;
      } else {
        On = true;
      }
    }
  }

  if (On == true) {
    xAxis();
    yAxis();
    zAxis();
    Serial.println("Data Sent.");
    delay(1000);
  }
  if (On == false) {
    shutDown();
  }
}

//Control of rotation about the Z axis
void zAxis() {
  InputZ = myIMU.readFloatGyroZ();
  myPIDZ.Compute();
  PWMZ = 127 + OutputZ;
  analogWrite(ZAxis, PWMZ);
}

//Control of rotation about the X axis
void xAxis() {
  InputX = myIMU.readFloatGyroX();
  myPIDX.Compute();
  if (OutputX < 0) {
    analogWrite(CLKWiseX, 0);
    analogWrite(AntiCLKWiseX, abs(OutputX));
  }
  if (OutputX > 0) {
    analogWrite(AntiCLKWiseX, 0);
    analogWrite(CLKWiseX, OutputX);
  } else {
    analogWrite(CLKWiseX, 0);
    analogWrite(AntiCLKWiseX, 0);
  }
}

//Control of rotation about the Y axis
void yAxis() {
  InputY = myIMU.readFloatGyroY();
  myPIDY.Compute();
  if (OutputY < 0) {
    analogWrite(CLKWiseY, 0);
    analogWrite(AntiCLKWiseY, abs(OutputY));
  }
  if (OutputY > 0) {
    analogWrite(AntiCLKWiseY, 0);
    analogWrite(CLKWiseY, OutputY);
  } else {
    analogWrite(CLKWiseY, 0);
    analogWrite(AntiCLKWiseY, 0);
  }
}

//Turn off all connected devices.
void shutDown() {
  analogWrite(CLKWiseX, 0);
  analogWrite(AntiCLKWiseX, 0);
  analogWrite(CLKWiseY, 0);
  analogWrite(AntiCLKWiseY, 0);
  analogWrite(ZAxis, 0);
}

Where can I get the <PID_v1.h> library?
Is the board library “Seeed nRF52 mbed-enabled Borads 2.7.2”?

The PID libray can be found here, <PID_v1.h> and yes.

The number of PWMs that can be used simultaneously appears to be 4.
It may be possible to increase this number by directly ssetting the registers.

Thank you, would you be able to point me in the right direction to get started?

You can find the manual at the following link
“Technical Documentation”

There are 4 output channels PSEL.OUT(0)-PSEL.OUT(3) for each PWM unit.
See “6.17 PWM - Pulse width modulation Figure 74: PWM module”

There are 4 PWM units, PWM0-3.
See “6.17.5 Registers”.

Assign GPIOs to the 4 output channels of 4 PWM units.
Refer to “6.17.5.23 PSEL.OUT[n] (n=0…3)”.

Up to 16 PWM channels should be available.

The function analogWritte() is written in the following file. The final output is “pwm->write(percent);”.
“C:\Users\UserName\AppData\Local\Arduino15\packages\Seeeduino\hardware\mbed\2.7.2\cores\arduino\wiring_analog.cpp : LINE45 or LINE58”

I am not a software engineer, so this is all I can tell you.

[EDIT] Using “Seeed nRF52 Borads 1.0.0” as the board library, I was able to output PWM on D0-D10 simultaneously.
If you use this board library, you may find my comments in the following link helpful.

1 Like

Thanks for the help, I ended up using the Seeed NRF52 Boards 1.0.0 library and scrapped the Bluetooth implementation as it was not necessary. Thanks again.