Xiao IO expander COMING, and Going.. Roll your own. ✌

Hi there,
I’m Glad they are looking at the whole expansion IO capability, For me as long as they don’t engineer it closed then I think it will be great!
They should always error on the side of MORE not LESS. IMO.
The B2B connector on the XIAO was a Happy day for me to see the possibilities it can lead to and make using Xiao really flexible.

I would be ok with a slight increase ,($1) IF so on the price even though the connector is less than that.
I need 4 or five for a project, but I am NOT buying cameras with them to just chuck in a drawer and never use. They need to either make them with it as is or add a new SKU#
I’ll inquire on the discord as well.

GL :slight_smile: PJ
:v: