XIAO Grove Expansion Board Case!

Hi there,

Nice :+1: I got some HIGH sides on these, I’m thinking a cover with the display in it (on Top)
the one on the right has bigger battery compartment too.

The one on the left , if i make the socket a little TAD shorter it will all fit. :+1:

GL :slight_smile: PJ :v:


yea, pen has a bubble level in it… :sunglasses:

Hi there,

I will post it up to m y thingiverse , time permitting…
But here is a ZIP file of the edited , printable parts for Grove Expansion Board Holder.

  • Added Feet
  • upsized the Sides
  • made a front cover
  • added some Seeed


END_CAP_Xiao_Grove.zip (1.7 MB)
Xiao_expansion_grove_base_End_cover.zip (609.7 KB)

HTH

GL :slight_smile: PJ :v:

Get you some Seeed Green PLA + and have a go at it.
You can adjust size in the slicer too. the Freecad files are there as well. ENJOY :+1: