XIAO + Expansion - Couple simple questions from a new user

HI

I have just got a XIAO + Expansion Board. I am new to this device and a very novice Arduino programmer

Couple of questions if anyone would be so kind as to answer please?

  1. When I run an Arduino I2c scanner on the Xiao when it is connected to the expansion i get 2 devices found…the first at 0x3c which I am guessing is the onboard OLED? The second is at 0x51 - what is this device?

  2. if i install Circuit Python on the Xiao & then want to return back to Arduino how do i do this? The wiki only seems to tell me how to install Circuit Python not how to return to Arduino

It is the RTC.

{ 0x51, “PCF2129A RTC” }

Hi Reivilo

Nice to meet you - even if only in the virtual sense!!

many thanks for that info - will add it to my rapidly growing Xiao knowledgebase

Hi dsssssssss9

You just open the Arduino IDE then upload any programme, it will back to Arduino mode.

Best regards
fenyi

Hi feny

Very kind of you to take the time to let me know… I really appreciate it

TTFN

DSSSSSSSSS(