Xiao ESP32S3 sense 基于micro python WIFI图传

话不多说,先上代码:

import camera
import time
import network
import socket


WIFI = network.WLAN(network.STA_IF)

'''
camera.framesize()参数:分辨率范围
1:FRAME_96X96 - 96x96 像素
2:FRAME_QQVGA - 160x120 像素 (QQVGA代表Quarter Quarter VGA)
3:FRAME_QCIF - 176x144 像素 (QCIF代表Quarter CIF)
4:FRAME_HQVGA - 240x160 像素 (HQVGA代表Half Quarter VGA)
5:FRAME_240X240 - 240x240 像素
6:FRAME_QVGA - 320x240 像素 (QVGA代表Quarter VGA)
7:FRAME_CIF - 352x288 像素 (CIF代表Common Intermediate Format)
8:FRAME_HVGA - 480x320 像素 (HVGA代表Half VGA)
9:FRAME_VGA - 640x480 像素 (VGA代表Video Graphics Array)
10:FRAME_SVGA - 800x600 像素 (SVGA代表Super VGA)
11:FRAME_XGA - 1024x768 像素 (XGA代表Extended Graphics Array)
12:FRAME_HD - 1280x720 像素 (HD代表High Definition)
13:FRAME_SXGA - 1280x1024 像素 (SXGA代表Super XGA)
14:FRAME_UXGA - 1600x1200 像素 (UXGA代表Ultra XGA)
15:FRAME_FHD - 1920x1080 像素 (FHD代表Full High Definition)
16:FRAME_P_HD - 1600x1200 像素 (P_HD代表Partial High Definition)
17:FRAME_P_3MP - 2048x1536 像素 (P_3MP代表Partial 3 Megapixels)
18:FRAME_QXGA - 2048x1536 像素 (QXGA代表Quad Extended Graphics Array)
19:FRAME_QHD - 2560x1440 像素 (QHD代表Quad High Definition)
20:FRAME_WQXGA - 2560x1600 像素 (WQXGA代表Wide Quad Extended Graphics Array)
21:FRAME_P_FHD - 2560x1600 像素 (P_FHD代表Partial Full High Definition)
'''  
    
if WIFI.isconnected():
    print('WIFI已连接!')
    while 1:
        cam = camera.init() 	 	 #长时间初始化失败请手动重启
        print("cam:",cam)
        time.sleep(1.5)
        if cam:
            camera.framesize(6)    
            camera.contrast(2)       # 增加对比度
            camera.speffect(0)       # RGB彩色
            break
    wlan_inf = WIFI.ifconfig()
    HOST = wlan_inf[0]
    PORT = 8080
    print('在浏览器中输入以下地址查看视频:', wlan_inf[0] + f':{PORT}')
    
    s = socket.socket(socket.AF_INET, socket.SOCK_STREAM)
    s.setsockopt(socket.SOL_SOCKET, socket.SO_REUSEADDR, 1)
    s.bind((HOST, PORT))
    s.listen(5)
    
    s.setblocking(True)
    client, addr = s.accept()
    client.settimeout(2)  
    print ('成功连接到:', addr[0] + ':' + str(addr[1]))
    request = client.recv(1024).decode('utf-8')
    client.send("HTTP/1.1 200 OK\r\n"
    "Server: Tao\r\n"
    "Content-Type: multipart/x-mixed-replace;boundary=Tao\r\n"
    "Cache-Control: no-cache\r\n"
    "Pragma: no-cache\r\n\r\n".encode())
    
    while 1:
        img = camera.capture()
        if img == False:
            print(img)#长时间拍照失败请手动重启
            time.sleep(1.5)
        else:
            break
    while True:
        img = camera.capture()
        header = "--Tao\r\n" \
         "Content-Type: image/jpeg\r\n" \
         f"Content-Length: {len(img) + len('--Tao\r\n')}\r\n\r\n"
        
        client.send(header.encode())
        client.send(img)
else:
    WIFI.active(True)
    WIFI.connect('HiWiFi_5B4AC2', 'b8507123')

手搓Socket完成服务端,如果长时间拍照失败,需要点击板子上的重启按钮

Manually rub the Socket to complete the server. If the photo taking fails for a long time, you need to click the restart button on the board.
LOL, Nice.
GL :slight_smile: PJ :v:

After each photo can not use the Thonny software above the restart button, otherwise it will lead to unable to take photos, need to press the reset button on the board

Hi there,
Looks like it goes to sleep after , picture.?
What does the serial output look like?
GL :slight_smile: PJ
:v:

Micropython calls to the camera often require a reboot, which I think is normal
My English is not good, please give me more advice:)