I think it is not related to Wifi. I am using esphome and tried everything without the camera module setup (just Wifi), then I automatically have ~140µA when entering deep sleep (via esphome), but when the camera module is configured and connected it is ~90 mA in deep sleep. As it happens not automatically on entering deep sleep, I am looking for something I can do before it manually e.g. send an I2C message to the OV2640 or an internal API call.