Xiao esp32s3 sense camera sleep current

Sorry I’m late. Need some clarification here. The wiki shows the difference in low power consumption values for different peripherals. The intention is to illustrate how much the actual impact on low power consumption can vary when connecting different peripherals, so that users can decide whether to connect hardware based on the extent of this impact.

This means that when we measure low power consumption, it is tested in a scenario where the camera or SD card functionality is not initialized in the code, but the hardware expansion board module is connected. The power reference provided does not accurately reflect the power consumption when actually using features like the camera and SD card