esptool.py v3.3
Serial port COM40
Connecting…Traceback (most recent call last):
File “esptool.py”, line 5387, in
File “esptool.py”, line 5380, in _main
File “esptool.py”, line 4687, in main
File “esptool.py”, line 115, in get_default_connected_device
File “esptool.py”, line 664, in connect
File “esptool.py”, line 629, in _connect_attempt
File “esptool.py”, line 519, in sync
File “esptool.py”, line 458, in command
File “esptool.py”, line 421, in write
File “serial\serialwin32.py”, line 325, in write
serial.serialutil.SerialTimeoutException: Write timeout
[2408] Failed to execute script ‘esptool’ due to unhandled exception!
上传项目出错