Hi there,
For the Bow, Tie on this one…
I found this Tap to wake, well documented, and Tests very well. Not sure where it came from ? But works very well.
9.3uA
tap to wake.
#include <Adafruit_SPIFlash.h>
#include <LSM6DS3.h>
#include <nrf52840.h>
#include <Wire.h>
Adafruit_FlashTransport_QSPI flashTransport;
LSM6DS3 myIMU; // Default is I2C mode
void QSPIF_sleep(void)
{
flashTransport.begin();
flashTransport.runCommand(0xB9);
flashTransport.end();
}
void setupWakeUpInterrupt()
{
// Start with LSM6DS3 in disabled to save power
myIMU.settings.gyroEnabled = 0;
myIMU.settings.accelEnabled = 0;
myIMU.begin();
// Set up the accelerometer for Wake-up interrupt.
// Per the application note, use a two step set up to avoid spurious interrupts
// Set up values are from the application note, and then adjusted for minimum power
myIMU.writeRegister(LSM6DS3_ACC_GYRO_WAKE_UP_DUR, 0x00); // No duration
myIMU.writeRegister(LSM6DS3_ACC_GYRO_WAKE_UP_THS, 0x02); // Set wake-up threshold
myIMU.writeRegister(LSM6DS3_ACC_GYRO_TAP_CFG1, 0x80); // Enable interrupts and apply slope filter; latch mode disabled
myIMU.writeRegister(LSM6DS3_ACC_GYRO_CTRL1_XL, 0x70); // Turn on the accelerometer
// ODR_XL = 833 Hz, FS_XL = ±2 g
delay(4); // Delay time per application note
myIMU.writeRegister(LSM6DS3_ACC_GYRO_CTRL1_XL, 0xB0); // ODR_XL = 1.6 Hz
myIMU.writeRegister(LSM6DS3_ACC_GYRO_CTRL6_G, 0x10); // High-performance operating mode disabled for accelerometer
myIMU.writeRegister(LSM6DS3_ACC_GYRO_MD1_CFG, 0x20); // Wake-up interrupt driven to INT1 pin
// Set up the sense mechanism to generate the DETECT signal to wake from system_off
// No need to attach a handler, if just waking with the GPIO input.
pinMode(PIN_LSM6DS3TR_C_INT1, INPUT_PULLDOWN_SENSE);
return;
}
void setup()
{
// Serial.begin(9600);
// delay(3000); //relax...
// Serial.println();
// Serial.println("Processor came out of reset.\n");
pinMode(LED_RED, OUTPUT);
pinMode(LED_GREEN, OUTPUT);
digitalWrite(LED_RED, HIGH);
digitalWrite(LED_GREEN, HIGH);
QSPIF_sleep();
// Flash green to see power on, reset, and wake from system_off
digitalWrite(LED_GREEN, LOW);
delay(1000);
digitalWrite(LED_GREEN, HIGH);;
// Minimizes power when bluetooth is used
NRF_POWER->DCDCEN = 1;
}
void loop()
{
// FreeRTOS will automatically put the system in system_on sleep mode here
delay(10000); // Measure idle loop power during this period
// Flash red before system_off sleep
digitalWrite(LED_RED, LOW);
delay(500);
digitalWrite(LED_RED, HIGH);;
// Setup up double tap interrupt to wake back up
setupWakeUpInterrupt();
// Execution should not go beyond this
NRF_POWER->SYSTEMOFF = 1;
}
power -ON
High-lighted is Sleep w/tap to wake…
SLeep w/ Tap to Wake ![]()
basic cycle 2 taps:
Basic single cycle with ONE tap
![]()
HTH
GL
PJ ![]()