XIAO BLE Sense battery level and charging status

Hi!
Is this assuming that the battery’s BAT+ BAT- are connected to the respective BAT+ BAT- pads on the back of the XIAO Sense for this driver to work? I’m currently using an “external” PMU for my 3.7V LiPo battery (Solar_Power_Manager_5V_SKU__DFR0559-DFRobot) and it has a dedicated BAT analog pin for battery voltage monitoring. Can I instead connect this BAT pin to the XIAO’S BAT+ pad? Thanks in advance.