In the context of electronic devices or development boards, such as the micro:bit or Arduino, there can be a difference between the 5V pin on the top side and the Vin (Voltage In) pin on the verso side. Here’s an explanation of their typical functions:
- 5V Pin: The 5V pin on the top side of a development board provides a regulated 5-volt power supply. It is generally used tiktok mp3 download to power external components or sensors that require a 5V power source. This pin provides a constant voltage output of 5 volts.
- Vin Pin: The Vin (Voltage In) pin on the verso side of a development board is typically used to supply power to the board itself. It is an input pin that accepts a range of voltages, often around 7 to 12 volts. The Vin pin allows you to power the board using an external power source, such as a battery or a regulated power supply. The voltage on the Vin pin is typically regulated down to the appropriate levels needed by the board’s components.