Hi all,
I have created a toolless, hardwareless and supportless, 14gram filament housing.
You can download it here:
Don’t hesitate if you have any questions!
Hi all,
I have created a toolless, hardwareless and supportless, 14gram filament housing.
You can download it here:
Don’t hesitate if you have any questions!
That is amazing!!! Happy to see it in use ![]()
Hi there,
Yes, You got a good one right here, as is or I would make these suggestions.
GL
PJ ![]()
omg… you are going to need a new shelf… elf
I can make a v2. How much wider should it be? do you have a sketch or example what you mean with the LED?
Hi there,
I stretched it (scale) in the slicer
![]()
What I printed was originally (no logo) 21.49mm. on your X,(I printed standing with supports and a Brim) and then "PHATTY "26.5mm wide on the mod for the small battery.
The Center section , can be hollow and make an access hole into it ![]()
Lose the dovetail in the front. (keeps it cleaner) Make the TOP slide out to the rear also is better. ![]()
You could turn the WHOLE Xiao 90 degrees and access the Buttons with plastic Paddle buttons in the LID(side), ![]()
The side walls need to be sturdier.. too thin on the STL above, I printed, Initially (first set of pics) Battery fits either orientation with stretched side, I increased wall thickness as well.
It’s a great Idea, to have a ready to Go, a Code ready Nugget for deployment. “Batteries Included”
![]()
HTH
GL
PJ ![]()