Hello,
Got my Wio-Terminal a few days ago and had a lot of fun playing around with it. I accidentally flashed a wrong bootloader-update(uf2) in an attempt to make games from arcade.makecode.com work. The device still works and provides a mass storage device when going into bootloader-mode but doesn’t do when not. (which the wio-terminal bootloader did even without being in bootloader-mode) Is there any way or binary around to flash it back? At INFO_UF2.TXT (ARCD-D51) it identifies as follows: UF2 Bootloader v3.2.2 SFHWRO Model: Feather Arcade D51 Board-ID: SAMD51J19A-Feather-Arcade-D51 I’m using Ubuntu x86_64 and didn’t yet manage to compile successfully from .
thanks
jackyjoy