Hi,
I have got following components:
- WM1302 Pi Hat for Raspberry Pi
- LoRaWAN Gateway Module WM1302
I’m referring LoRaWAN® Gateway Module WM1302 - Seeed Wiki to get started but I don’t find any information about connecting GPS and LoRa antenna. Are there any specific sockets on Pi Hat or GW module for connecting GPS and LoRa antenna?
Yes, I have the same question. There doesn’t seem to be any information on antenna connections. I assume the GPS module sent with the Pi Hat connects to the U.FL connector on the Pi Hat labeled ANT. On the WM1302 Mini-PCIe board, there is also a U.FL connector labeled RFIO and pads labeled RFI – can I add a simple wire antenna to these pads, and if so where? Also, is there a U.FL mating antenna kit available for the US915 band?
i recently acquired pi hat and was wondering which port to plug into as well. did you find out?
The port on the hat is for the GPS antenna