Wio Terminal Battery Chassis Does Not Work X 2

At the same time, you can also refer to the working indicator of the battery to judge the current working state of the battery.

Green LED: Light On is mean the board charing.

Red LED: Light on is mean the OTG(battery discharge) enable.

Yellow LED: Light on is mean the male interface output/input 5V.

The best way is to test the battery level to determine whether it is not working due to lack of power.