Wio Terminal Arduino upload problem on MacBook

I have tried to upload my first Arduino sketch to the Wio terminal from my MacBook and am getting a java permissions error when it tries to upload, even though the correct USB device is shown. Help please.

java.io.IOException: Cannot run program “/Users/Tony/Library/Arduino15/packages/Seeeduino/tools/bossac/1.8.0-48-gb176eee/bossac”: error=13, Permission denied
at java.lang.ProcessBuilder.start(ProcessBuilder.java:1048)
at java.lang.Runtime.exec(Runtime.java:620)
at java.lang.Runtime.exec(Runtime.java:485)
at processing.app.helpers.ProcessUtils.exec(ProcessUtils.java:11)
at cc.arduino.packages.Uploader.executeUploadCommand(Uploader.java:129)
at cc.arduino.packages.uploaders.SerialUploader.runCommand(SerialUploader.java:383)
at cc.arduino.packages.uploaders.SerialUploader.uploadUsingPreferences(SerialUploader.java:197)
at cc.arduino.UploaderUtils.upload(UploaderUtils.java:77)
at processing.app.SketchController.upload(SketchController.java:732)
at processing.app.SketchController.exportApplet(SketchController.java:703)
at processing.app.Editor$UploadHandler.run(Editor.java:2055)
at java.lang.Thread.run(Thread.java:748)
Caused by: java.io.IOException: error=13, Permission denied
at java.lang.UNIXProcess.forkAndExec(Native Method)
at java.lang.UNIXProcess.(UNIXProcess.java:247)
at java.lang.ProcessImpl.start(ProcessImpl.java:134)
at java.lang.ProcessBuilder.start(ProcessBuilder.java:1029)
… 11 more
An error occurred while uploading the sketch

You can refer to the solution here for a solution.

Thank you @Citric - that was the solution, although I have no idea why a file appeared in my Arduino library without the correct permissions.