Hi @Iakshan,
I’m happy to see that you are searching the cause and I’m sure you’ll find it soon.
My investigations let me think that it might be a similar reason as posted here:
At least if I add a ‘_connected = false’ in the WiFiClientSecure::stop() routine, my application continues to work after a failed upload.
(However it may be that the true cause is somewhere else)
Best regards
RoSchmi
Good news !! Now with new RTL8720 firmware (seeed-ambd-firmware) v2.1.1 in a new test run until now 650 successful uploads (https) and still running. There was one failed upload (is expected to can happen) but the program continued to perform successive uploads as expected. Watchdog was not activated.
Unfortunately I was happy too early. Stopping of uploads seems to occure now much less often but very rarely my App still stops uploading (all subsequent push request return with error code -1) while the loop is still running.
Does it work endlessly on your side with firmware v2.2.1?
Hi @RoSchmi,
Could you try changing the delay value here Seeed_Arduino_rpcUnified > src > erpc > erpc_arduino_uart_transport.cpp (line 299) on your end and test it? The delay seems to be the issue. When the delay is too high, it seems to be slow, and when the delay is too low, it seems to be unstable.
Thanks, I’ll try, actually 5 ms delay.
BtW: Is there a way to reset the MCU -> RTL8720 connection without rebooting the complete board. So one could start a retry of the ssl transmission and would not loose data in ram.
Thanks @lakshan . Unfortunately this code alone didn’t work to recover the connection. Probably it would also be needed to reinitialize the serial port of the SAMD51 MCU.
I think it would be too difficult to find out how this could be done.
Best Regards
RoSchmi
Thanks @lakshan, I’m not sure which code you mean with:
However, before trying this I would like to rule out that there is a memory leak causing the issue.
Do you have some routines which you use on the SAMD51 to test for memory leaks?
I think, that I have already found some code;
Edit: The code I posted here before didn’t work for me as expected.
Now I’m using this code in my loop to check if there is a memory leak:
(depends on rpcWiFi library)
Edit2: Using pvPortMalloc() is not correct, malloc() has to be used, code is corrected
// Keep track of tries to insert and check for memory leak
insertCounterAnalogTable++;
uint32_t * ptr_one = (uint32_t *)malloc(100);
free(ptr_one);
if (insertCounterAnalogTable == 1)
{
referenceHeapAddr = (uint32_t)ptr_one;
}
lostLeakageBytes = (uint32_t)ptr_one - referenceHeapAddr;
char buf[25] {0};
sprintf(buf, "Allocating at: %10X", (unsigned int)ptr_one);
Serial.println(buf);
sprintf(buf, " Lost %i", lostLeakageBytes);
Serial.println(buf);
Hi @lakshan,
I made tests with 5ms and 6ms delay. Didn’t solve the issue.
In my application it is not needed to store data in Ram permanently, so I can use the watchdog or reboot after a failed upload. With these measures I can do my uploads permanently. For other applications I will have to wait on your team to solve the problem.
Best Regards
RoSchmi
Actually my App is running flawlessly (delay 4 ms) for 9 hours without using the watchdog, that’s a new record !! It’s a pity that I have to stop it now to continue programming.
Did you make any changes in the rpcUnified library update of yesterday which could have been a game changer?
I still have no other serious applications. If I had an idea of an internet using App which has the need of keeping data in the Ram I would not start before the platform has proved to run stable over longer periods of time.
Hi @lakshan,
problem still not completely solved. My App very seldom stops to upload even with 20 ms delay. Sometimes several hundred successful uploads but then one upload fails and the drivers seems not to be able to recover from such an anexpected situation. I’ll try @stevedb 's suggestion tomorrow.
Best Regards
RoSchmi
Hi, with stevedb 's suggestion with 100us delay as mentioned -> malfunction after 129 successful uploads. The 130. try to upload (post request) returned with error code -1, on the next try to upload the App crashed (loop stopped running).
BtW: You are using a baudrate of 1.843.200. Did you try using a lower baudrate?
Still the same problems. Occasinally my App hangs an requires reset by the watchdog, occasionally https requests fail and the system doesn’t recover from this situation. Is the Seeed team still trying to fix/improve the WiFi associated libraries?