Wio LTE HTTP REQUEST

Hi. I have an HTTP post Sketch that work for my ESP32 wifi project, however I’m trying to adapt the sketch to a Wio LTE. I can reach the server however it’s not creating any registry. Can someone help with the missing piece? Thanks

Esp 32 Sketch:

#include <WiFi.h>
#include <HTTPClient.h>
#include <M5Atom.h>


// Replace with your network credentials
const char* ssid     = "Wifi XXXXX";
const char* password = "XXXXXXX";


// REPLACE with your Domain name and URL path or IP address with path
const char* serverName = "http://datalogger.equione.pt/post-esp-data-pos.php";

// Keep this API Key value to be compatible with the PHP code provided in the project page. 
// If you change the apiKeyValue value, the PHP file /post-esp-data.php also needs to have the same key 
String apiKeyValue = "YYYYYYY";



String apiKeyValue = "tPmAT5Ab3j7F9";
String sensor = "94:B9:7E:A8:E2:7C";
float temp_ambiente = 12.4;
float temp_interior = 5.6;
float voltage = 0.00;
float current = 0.00;
float power = 0.00;
float energy;
float frequency;
float pf;


void setup() {
  // put your setup code here, to run once:

M5.begin();
  Serial.begin(115200);
  WiFi.begin(ssid, password);
      Serial.println("Connecting");
      while(WiFi.status() != WL_CONNECTED) { 
      delay(500);
      Serial.print(".");
      }
      Serial.println("");
      Serial.print("Connected to WiFi network with IP Address: ");
      Serial.println(WiFi.localIP());
        delay(20);


}

void loop() {
  // put your main code here, to run repeatedly:


 //ENVIAR PARA SERVIDOR VIA WiFi
              
      if(WiFi.status()== WL_CONNECTED){
       HTTPClient http;
    
    // Your Domain name with URL path or IP address with path
    http.begin(serverName);
    
    // Specify content-type header
    http.addHeader("Content-Type", "application/x-www-form-urlencoded");
    
    // Prepare your HTTP POST request data
    




    
    String httpRequestData = "api_key=" + apiKeyValue + "&sensor=" + sensor
                          + "&ambiente=" + temp_ambiente + "&interior=" + temp_interior
                          + "&voltagem=" + voltage + "&amperagem=" + current + "&potencia=" + power + "";
    

    
    
    Serial.print("httpRequestData: ");
    Serial.println(httpRequestData);
    

  // Send HTTP POST request
    int httpResponseCode = http.POST(httpRequestData);
      if (httpResponseCode>0) {
      Serial.print("HTTP Response code: ");
      Serial.println(httpResponseCode);
    }
    else {
      Serial.print("Error code: ");
      Serial.println(httpResponseCode);
    }
    // Free resources
    http.end();
    
  }



}

Wio LTE Sketch:

#include <WioLTEforArduino.h>
#include <stdio.h>

#define URL "http://datalogger.equione.pt/post-esp-data-pos.php"



#define APN               "myconnection"
#define USERNAME          ""
#define PASSWORD          ""


String apiKeyValue = "tPmAT5Ab3j7F9";
String sensor = "94:B9:7E:A8:E2:7C";
float temp_ambiente = 12.4;
float temp_interior = 5.6;
float voltage = 0.00;
float current = 0.00;
float power = 0.00;
float energy;
float frequency;
float pf;


#define INTERVAL          (10000)

WioLTE Wio;

// ---------------------------------------------------------------
void setup() {
  SerialUSB.println("### I/O Initialize.");
  Wio.Init();
  
  SerialUSB.println("### Power supply ON.");
  Wio.PowerSupplyLTE(true);
  delay(500);

  SerialUSB.println("### Turn on or reset.");
  if (!Wio.TurnOnOrReset()) {
    SerialUSB.println("### ERROR! ###");
    return;
  }

  SerialUSB.println("### Connecting to \""APN"\".");
  if (!Wio.Activate(APN, USERNAME, PASSWORD)) {
    SerialUSB.println("### ERROR! ###");
    return;
  }

  SerialUSB.println("### Setup completed.");
}

// ---------------------------------------------------------------


void loop() {
     char data[200];
    int status;

    SerialUSB.println("### Post.");
    sprintf(data, "api_key=%s&sensor=%s&ambiente=%.2f&interior=%.2f&voltagem=%.2f&amperagem=%.2f&potencia=%.2f", apiKeyValue.c_str(), sensor.c_str(), temp_ambiente, temp_interior, voltage, current, power);
    

    SerialUSB.print("Post:");
    SerialUSB.print(data);
    SerialUSB.println("");
    if (!Wio.HttpPost(URL, data, &status)) {
        SerialUSB.println("### ERROR! HttpPost ###");
    }
else
    {
    SerialUSB.print("Status: ");
    SerialUSB.println(status);
    }   

    SerialUSB.println("### Wait.");
    delay(INTERVAL);
}