I configured the system and the Arduino IDE as instructed. Then I ran the default RSSI reporting example of the Wio LTE Cat M1/NB-IoT board. However, the board keeps outputing “.” at the serial port. In other words, the SARA module is not alive.
Do you have any suggestion?
Thanks.
MAKE A BACKUP FIRST!
Then in ublox_sara_r4.cpp (in library src) try changing PowerOn() to:
void Ublox_sara_r4::powerOn(void)
{
init_AtTransport();
// Enable power to the module
pinMode(MODULE_PWR_PIN, OUTPUT);
digitalWrite(MODULE_PWR_PIN, HIGH);
// Pause a bit to allow power to come up
delay(100);
// Assert PowerKey pin for just over 3.2 seconds
pinMode(PWR_KEY_PIN, OUTPUT);
digitalWrite(PWR_KEY_PIN, HIGH);
delay(3500);
digitalWrite(PWR_KEY_PIN, LOW);
// Pause at short while
delay(200);
// Assert it again for just under a second
digitalWrite(PWR_KEY_PIN, HIGH);
delay(800);
digitalWrite(PWR_KEY_PIN, LOW);
// Set RTS pin low to enable UART communication
pinMode(RTS_PIN, OUTPUT);
digitalWrite(RTS_PIN, LOW);
}
Regards
-Bill K
R O SoftWare