WiKi Addition for wireless connectivity and ArduPy

There are WiFi/BLE Connectivities but there no introduction of their usage in the wiki. Could you please add the description about this?
In addition, it could be better to add the description or link to the transfer syntax from the Arduino Library to the MicroPython library.

These software are converted to get and you can see that we are very successful. The documentation is being edited and internally reviewed, and we want to make sure that everyone can easily use the A heat P has. @ONLYA

Did you find a way to make Wi-Fi connectivity work while using ArduPy?

Sadly, I cannot find a way to use WiFi + BLE connectivity on both Ardupy and CircuitPython. But it worth me to write a convertable external C module for the Micropython from the wireless connectivity library and integrate it into Ardupy while compiling the binary…
Now, I think this product is not a device for simple IoT usage yet, still an offline device itself. I suppose that the devs are developing those features. @giorgiomassa @Baozhu