Wifi very unstable

I am struggling to get a good wifi connection on the esp32s3. I have now “concluded” it’s a hardware problem. I have tried multiple esp32s3 with similar results. The same code runs absolutely fine on xiao esp32c3 (but I need more memory).
I have run both esp idf code, arduino code, with all sorts of different configurations, including various antennas.
If I use NVS at the same time as wifi, then wifi never connects.
This is very disappointing. Oh, I forgot, I also tried multiple different antennas, with no result. As some have pointed out, touching the antenna can temporarily solve the problem.

How about lowering the transmit power?
The default is 20, but my latest XIAO-ESP32S3 worked stably when I set it to the minimum of 10.

start idf.py menuconfig
find TX_POWER
and change TX_POWER value.

after that check sdkconfig file.

CONFIG_ESP_PHY_MAX_WIFI_TX_POWER=10
CONFIG_ESP_PHY_MAX_TX_POWER=10