When I connected the wifi module from wave share ( AC8265 Wireless NIC for Jetson Nano, WiFi / Bluetooth ) it was not detected on the board the module placed back into the original board from NVIDIA. The wifi and bluetooth work perfectly. do i have to reimage the card for the J202 board to get the wifi module to work or should it work with the image that works on the Nvidia original board. or is the CAN bus interfering with the board how do i disable the CAN bus on the board so the wifi module will work