Hi all,
I appear to have bricked my new BBGW (editing the demo script /boot/uEnv.txt as described in the doc, so that it no longer completes the boot process).
I don’t have a 3.3V serial adapter handy, so I’m trying to get the unit to boot from a USB stick to re-edit the start-up script.
Is there a source on-line for the actual boot image that comes pre-loaded on the BBGW device (and starts up running the WiFi web and Cloud9 servers, and exports a mountable file system to USB)?
If there is, can one write this to a USB stick and boot the BBGW that way?
…any reply appreciated…
stp in SB/CA
Thanks for your response, but if I boot the default image,
<LINK_TEXT text=“https://debian.beagleboard.org/images/b … 07-4gb.img”>https://debian.beagleboard.org/images/bone-debian-9.5-iot-armhf-2018-10-07-4gb.img</LINK_TEXT>
it doesn’t start the WiFi services or the LED-flashing demo.
Is there a source for the actual image that comes pre-installed on the BBGW?
stp
Hi there,
I uploaded the factory image to google driver. please download and test. thanks.
<LINK_TEXT text=“https://drive.google.com/open?id=1fmon- … znXRFm1UmP”>https://drive.google.com/open?id=1fmon-NYv68hTcsNMLU_c7UznXRFm1UmP</LINK_TEXT>
Many Thanks !!