I know they are compatible because the flashing step in the Arduino IDE uses the adafruit-nrfutil command. However, there’s currently no support for the Xiao BLE/BLE Sense in the upstream project.
I’d prefer to flash my own bootloader, but i don’t wanna screw it up.
So are there any differences between the upstream version and the one onboard other than lack of upstream contribution of the proper board file?
I would appreciate if you folks would contribute your changes to the upstream project.
Also, the default offset is different: 0x27000 instead of 0x26000 for the application start area. Why is that? is it just to leave room for say device stored settings?