Hi,
I have purchased a ReSpeaker 6 microphone array for the Raspberry Pi but am struggling to determine what speakers to use, I know they are a JST2.0 connection but when I search on Amazon I see 3W 8 Ohm, 5W 8Ohm and I read somewhere that the maximum on the ReSpeaker was a 1W.
Does anyone have a definitive answer on what speaker power levels are compatible with the ReSpeaker as I don’t want to damage it.
Thanks for your help.
In case anyone is interested, I bought these off Amazon:
CQRobot Speaker 3 Watt 4 Ohm Compatible With Arduino Motherboard, JST-PH2.0 Interface. It is Ideal for a Variety of Small Electronic Projects. https://www.amazon.co.uk/dp/B0822Z4LPH/ref=cm_sw_r_cp_api_fabc_C3VJBGDA0PTJRSKSS1W7?_encoding=UTF8&psc=1
There’s 2 speakers but only one port on the ReSpeaker so you only use one, but I can confirm it works and sounds pretty good.