What j1010 gpio should i use for steering, speed, pololu multiplexer enable slave jetracer

what j1010 gpio should i use for steering, speed, pololu multiplexer enable slave jetracer

Hi there,
And welcome Here…
Just follow the wiki on it and test it.

Step 1: Download the pinmux document according to the SoM you are using. Here we choose the Jetson Orin NX/ Nano document

Step 2: Find the GPIO label (under Customer Usage column) corresponding to the Module Pin Name that we got before. For example, for GPIO12, it is GPIO3_PN.01 and here we refer to PN.01

Step 3: Enter the terminal of the Jetson device and execute this command

sudo sucat /sys/kernel/debug/gpio

Step 4: Find the GPIO number corresponding to the GPIO label that we got before

THE rest is HERE…

If you get stuck , come back and let us know. :+1:

HTH
GL :slight_smile: PJ :v: