What is the specification of OV2640 lens? XIAO-esp32s3 Sense

Hello,
I would like to know the lens specifications of the default camera OV2640 on the XIAO ESP32S3 Sense.

I am interested in information such as the ‘focal length’ and ‘focusing range’ of OV2640, but I cannot seem to find it.
Anyone knows where to find it?
I have only found the detailed parameter datasheet for the OV5640 in SeeedStudio wiki.

THANKS

Hi there,
G man says this about it,
What is the focal length of the lens OV2640?

Specifications

Specifications Parameters
Conventional view lens Focal length 4.8±5%mm Aperture 2.4±5% Lens type 1/4inch Field of view 65° Pixels 2M Reverberation <1% Sensor chip OV2640
Firmware default communication method UART: 115200bps 8N1

HTH
GL :slight_smile: PJ
:v: