Im trying to get 18 soil moisture sensors working off one Pi. So we are considering either of the following sensors although am leaning towards the capacitive version (first one):
Looks like we don’t have so many Grove mouth expanders yet… Or something else. My recommendation is that you connect all VCC together, GND together, and then use 18 GPIO ports to collect data. Go transforming wire so quite appropriate.
No, we use these expansion boards with Grove ports to complete these cases for the cleanliness of the wiring when we write the wiki. You can directly connect to the GPIO port on the Raspberry Pi to read data, and the rest of the content can also be operated according to the wiki.