What is the actual XIAO oscillator frequency

The XIAO Wiki “Specifications” says only: “…running at up to 48MHz”. But, what is the actual oscillator frequency? And what is the minimum number of clock cycles per instruction – like, for instance, a NOP?

Hi @Steve_Lawson,

XIAO uses the internal RC oscillator of the chip and the base frequency is 8MHz. It goes through a series of frequency divisions until 48MHz to work for SAMD21.

The NOP is 1/48MHz, which is about 0.02us.

Please check here for further details on the subject:

Best Regards,
Lakshantha