Hello, I am designing a product which includes a Wio-E5 (aka LoRa-E5) module.
In order to write the firmware on it, I need to know some details which are hard to find:
What is the exact partnumber of the STM32WLE inside this module. This is needed so in STM32CubeMx we can create the correct projects.
Does the module provide an external 32,768 kHz XTAL to the MCU, so we can run the RealTimeClock from that source ?
Is the MCU VBAT connected to VDD, so when we power the module with a battery, we can measure the battery voltage through ADC-VBAT
One more question : can you clarify something about the pin 24 : PB13
The datasheet mentions this pin as SPI2-CLK, which matches with the SMT32WLE datasheet, but it also mentions Boot pin (active low)
At first I thought this was the BOOT0 pin, to force the MCU into bootloader, but there are 2 strange things:
the BOOT0 pin is PH3 on the STM32WLE (not PB13).
to force bootloader, you need to bring the BOOT0 pin HIGH, not LOW.
So I need a bit more info about how this pin is working internally in the LoRa-E5 module
On the LoRa-E5 development board, the USB-SERIAL is connected to PB6/PB7 of UART1, which cannot be used for bootloading (STM32WLE can bootload from UART1 on pins PA9/PA10 or from UART2 on pins PA2/PA3).
So what does this BOOT button (pulling PB13 low) do ?