Hello, I have a Xiao ESP32C3 and I am trying to understand what the voltage of the 5V pin represents when the board is powered only via battery. Pinout available here
From my experiments, the 5V pin voltage is slightly above 5V when the board is powered via USB and there is no surprise there, especially given that the label on the pin is VUSB
If I instead disconnect the USB and only power the board from a battery (connected to the BAT + and BAT - pads) I have an unexpected voltage on the 5V pin. The voltage is not stable at all. I see it floating between 0.1V till 1.8V.
The voltage between the two battery pads is about 4V, which is sensible and tells me that the battery is fine. The 3V3 pin has the expected voltage as well, so again everything is fine on that front.
Is this expected? Is the 5V pin supposed to be used only when the device is powered via USB?
To add to my confusion, I also have an Adafruit QTPy ESP32C3 and on that board the voltage of its 5V pin is 3.75V, which sounds it could be the voltage of the battery minus the drop from a protection diode.
Is there a recommended way to power a device from battery instead of the 3V3 pin?
I can think of 2 options:
keep the battery connected to its pads and connect the device to BAT+. I’m not sure if this is safe when using USB to charge the battery.
use a separate battery charger and power both the other device and the Xiao (using the 5V pin + protection diode). This should be safe but involves additional components and “wastes” the charger in the xiao
HIGH on XIAO’s I/O is 3.3V. Is there a problem with the interface when 4V is supplied to the device?
What is the link to the device you are using? I think I can check the specs.
Thank you so much for your help. Really appreciated!
If I connect the battery to BAT+ do I need to add any protection diode or is a straight connection fine?
In my experiments I was using a Nordic PPK2 in source mode. In the initial experiment I connected it to the battery pads and then connected the device straight to the Xiao pins.
I then tried to do the same but connecting the device to the 5V pin, which is what led me to ask the initial question in this discussion.
That didn’t work so I got a breadboard out and used the PPK2 to power both the Xiao (using its 5V pin as the input) and the device.
As you can see in the link below, the sleep current of ESP32C3 is less than 50uA. if you have PPK2, you should check the current consumption of XIAO and display unit respectively.
The sleep current of the display unit chip is 3uA, so the rest might be the display panel and the boost circuit. Or maybe it is not sleeping properly.
The battery (connected to BAT+) typically goes to a Li-ion battery management IC, then to a 3.3V regulator.
The 5V pin (VUSB) is now disconnected from any valid power rail and is floating.
The random voltage (0.1V to 1.8V) you’re seeing is due to leakage currents or residual capacitance — it’s not usable power and not expected to be stable.