#WishList Product cooking time. We’re designing a Vehicle Monitoring Device based on a Seeed LoRa E5 and CAN Bus. With this module, you can build a LoRa sensor network where you can use the onboard CAN Bus to read the sensor data of the car and send the data back through LoRa. The device will come with the following features:
1⃣️ LoRa-E5 module
2⃣️ CAN Bus communication, MCP2515, and SN65HVD230
3⃣️ A variety of power supply methods, lithium battery, USB, and 7-28V DC input, as well as a solar panel input connector
4⃣️ USB to serial function, using USB to communicate with the board
5⃣️ Low-power design, the CAN Bus power on the board and the output power can be turned off through the MOS FET to save power
6⃣️ Two Grove connectors for easy access to the 300+ Grove modules
7⃣️ Optional u-FL and SMA antenna
Do you like this design? Shall we scale it up to make it available in our official store? What other features/IOs/functions that you’d love to add to this product? Any price suggestions? Shout-our your voices in this forum discussion:point_down:. Or if you prefer, feel free to join our Discord for a more in-depth discussion.
One more piece of good news for those who want to scale up your LoRa E5 projects, Seeed Fusion is running a LoRa E5 Sponsorship where you can apply to get 2 PCBA boards manufactured 100% completely FREE for your LoRa E5 design. Check out more: https://lnkd.in/gwD2SczF
Dear all, thank’s for inviting the community for feed back.
I’m running a small company which develops products for the sailing industry: modern sensors of any kind connected to CANbus (NMEA2000) found on almost all boats. Some sensors will be connected via Bluetooth Low Energy (BLE 5.2) to a central communications gateway. Thank’s to the very low power consuming footprint. We’re using Nordic Semiconductor’s nRF52 family.
So please can you add BLE 5.2 on the board. Many thanks in advance.
Hi Vojagxo! Thank you very much for your proposal. I have just communicated with our product manager that the function of BLE may not have much to do with the actual use scenario of my board, which will make the board more complicated. We will consider your opinion again! Have a great day!
Hi Sun, thank you for your answer. I understand your response very well. Integrating BLE makes the board too complicated and you will loose focus.
I’m convinced that the board will see high demand from the global market. The combination of ARM Cortex-M4 with CAN (MCP2515 and SN65HVD230) and LoRa is very attractive for many use cases - not only for vehicles…
Count me in as interested, I have been looking for something like this to troubleshoot cars and have some of that OB2 info on a display in the vehicle. Tell us what you want from us, we are not programmers but we can suggest, test, break and report back.
The test equipment out there that is under $1100 is too basic, we all need bi-directional communication on all available CAN Busses. Yes to GPS as well.
-c