Using the “Wio-SX1262 for XIAO” to easily build LoRa point-to-point communication with various XIAOs

For display, I was a bit surprised that some code I work with required no updates for this OLED and the Xiao expansion base… I was doubting pins where available, but it worked with the default code… one miracle in a string of pain getting the pin mapping for the rest of the setup!

I realize after looking harder, you used the newer Xiao SX1262 base rather than the meshtastic kit with the smaller sx1262 board… So that probably explains the difference.
Can it plug in to the expansion base?

1 Like