Using SEEED_GFX2 with SEEED_Driver_Board; (SKU 114993558); AND XIAO_ESP32C6

Hi there,

SO, Those don’t look like the first three lines of the compiler output, ???
more like the errors?

and you failed on the code tags portion :grin:
its at the top of the edit page header between the ""quotes and the UPLoad…
“</>” :backhand_index_pointing_left: that one, put your stuff in those, for maximum results.

In file included from c:\Users\gesch\Documents\Arduino\libraries\Seeed_GFX2\src/bus/Bus_SPI.h:15,
from c:\Users\gesch\Documents\Arduino\libraries\Seeed_GFX2\src/Seeed_GFX.h:54,
from C:\Users\gesch\Documents\Arduino\ePaper\gfx2_epaper_lines_text\gfx2_epaper_lines_text.ino:11:
c:\Users\gesch\Documents\Arduino\libraries\Seeed_GFX2\src/bus/Bus_SPI_Platform.h: In function ‘void seeed_gpio_lo(uint8_t)’:
c:\Users\gesch\Documents\Arduino\libraries\Seeed_GFX2\src/bus/Bus_SPI_Platform.h:86:32: error: no match for ‘operator=’ (operand types are ‘volatile gpio_out_w1tc_reg_t’ and ‘int’)
86 | GPIO.out_w1tc = (1 << pin);

Your close , try again.
HTH
GL :slight_smile: PJ :v:

This demo ,

uses the LM20A but same libs , so check out the code attached to the posts… Should show you something you are missing? Or Post your code using the code tags above and we can look. :+1:

or this one ,