I installed the IMX477 camera driver on my Jetson board, and after rebooting, none of the USB ports are working — both mouse and keyboard are unresponsive.
I can’t access the terminal or use SSH because input devices are not recognized at all.
Has anyone experienced this issue?
Is there a way to fix this without re-flashing the system?
Board: Jetson Orin NX
Jetpack: 6.2