Hi, i am new here, and my englisch is not so good.
I have bought the “Seeedstudio Grove - Starter Kit V1.1b” and an Arduino UNO.
I am totally new to this term and have some questions:
Can i use the Arduino UNO, the Seeedstudio Wifi Shield and the Motor Shield V1.0 together?
And this without loss of some of the Ports? (6xDigital, 5xAnalog, 1xUART, 1xIIC)
And whats about the LCD,
on the Motor Shield if i patch the Digital I/O jack on the first digital port and the LCD on the UART-port, is this working?
Because both have “D1” standing beneath them.
THX for the work, with this “Plug&Play”-System starting Arduino is easy!