Unbrick Wio Terminal

First off: cool product. I can see potential, however I wish for more docs with clearer examples (maybe I should write some?).

Unfortunately, I have bricked my Wio Terminal. How can I unbrick it?

My last aip flash did not complete successfully. Since then, Wio Terminal is a brick.

Green light comes on, but no USB connection.

“double-clicking” the on button does nothing special.

Not sure what to do next.

Any ideas?

Try double clicking the power switch very quickly, the Blue led should blink up in a way like this:

Anson家威 2020-05-05 09.09.05.2020-05-12 09_09_43

and see if usb port appears.

I see blue light flashing, but no USB connection.

$ aip board
ERROR: Sorry, the device you should have is not plugged in.

Hi @golden,

when blue light flashing, flash an Arduino Program into it first.

Ley say, flash a Blink example into the Wio Terminal first. Then, can use aip tp flash the ardupy firmware.

USB is not working.

How do I flash, if I cannot connect via USB?

when double clicking, can you see this:

image

I am on a Mac.

I do not see /dev/cu.usbmodem401301 as I did earlier - before flash.

This was flash error:

 wio-terminal aip list
Package                        Version Location
------------------------------ ------- ------------------------------------------------------------------
seeed-ardupy-ultrasonic-sensor 1.0.0   https://github.com/Seeed-Studio/seeed-ardupy-ultrasonic-sensor.git                                                                            /7.1s
➜  wio-terminal aip build
QSTR updated
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-gcc  -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -U_FORTIFY_SOURCE -Os   -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/foantcyemod_ardupy_ultrasonic_sensor.c.o   -c /Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/mod_ardupy_ultrasonic_sensor.c
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-g++  -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu++11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -fno-rtti -fno-exceptions -fno-threadsafe-statics -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -std=gnu99 -U_FORTIFY_SOURCE -Os   -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/oxtbkgdqwrapper_ultrasonic_sensor_hal.cpp.o   -c /Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/wrapper_ultrasonic_sensor_hal.cpp
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-g++  -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu++11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -fno-rtti -fno-exceptions -fno-threadsafe-statics -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -std=gnu99 -U_FORTIFY_SOURCE -Os   -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/fsjowbnuUltrasonic.cpp.o   -c /Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor/Ultrasonic.cpp
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-gcc  -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -U_FORTIFY_SOURCE -Os   -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/leduwjsmobjmodule.c.o   -c /Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/py/objmodule.c
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-gcc  -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -U_FORTIFY_SOURCE -Os   -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/fxqrvjwuparse.c.o   -c /Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/py/parse.c
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-gcc  -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -U_FORTIFY_SOURCE -Os   -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/hqaefmntqstr.c.o   -c /Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/py/qstr.c
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-gcc  -DARDUINO=10810 -DARDUINO_ARCH_SAMD -DWIO_TERMINAL -DARDUPY_MODULE -DARM_MATH_CM4 -DENABLE_CACHE -DF_CPU=120000000L -DUSBCON -DUSB_CONFIG_POWER=100 -DUSB_MANUFACTURER="Seeed Studio" -DUSB_PID=0x802D -DUSB_PRODUCT="Seeed Grove UI Wireles" -DUSB_VID=0x2886 -DVARIANT_QSPI_BAUD_DEFAULT=50000000 -D__FPU_PRESENT -D__SAMD51P19A__ -D__SAMD51__ -I/Users/golden/.config/aip/ardupycore/ArduPy -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/lib/lwip/src/include -I/Users/golden/.config/aip/ardupycore/ArduPy/MicroPython/extmod/lwip-include -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core/tinyusb/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/cores/arduino/Adafruit_TinyUSB_Core -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Wire -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SPI -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/Adafruit_ZeroDMA -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/variants/grove_ui_wireless -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/core/arduino/USB -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/HID -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/USBHost/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/hardware/samd/1.7.1/libraries/SAMD_AnalogCorrection/src -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Include -I/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS-Atmel/1.2.0/CMSIS/Device/ATMEL -I/Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor -I/Users/golden/.config/aip/modules/seeed-ardupy-ultrasonic-sensor/Seeed_Arduino_UltrasonicSensor -I/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri -mcpu=cortex-m4 -mthumb -c -g -w -std=gnu11 -ffunction-sections -fdata-sections -nostdlib -mfloat-abi=hard -mfpu=fpv4-sp-d16 -MMD -g -Wall -Werror -Wpointer-arith -Wuninitialized -Wno-unused-label -U_FORTIFY_SOURCE -Os   -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/wahfyevd__init__.c.o   -c /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/__init__.c
/Users/golden/.config/aip/ardupycore/Seeeduino/tools/arm-none-eabi-gcc/bin/arm-none-eabi-gcc  -L/Users/golden/.config/aip/ardupycore/Seeeduino/tools/CMSIS/4.5.0/CMSIS/Lib/GCC -Os -Wl,--gc-sections -save-temps -T /Users/golden/.config/aip/ardupycore/ArduPy/boards/wio_terminal/flash_with_bootloader.ld -Wl,-Map,/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/firmware.map -Wl,--whole-archive /Users/golden/.config/aip/ardupycore/ArduPy/lib/libmicropython.a -Wl,--no-whole-archive /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/foantcyemod_ardupy_ultrasonic_sensor.c.o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/oxtbkgdqwrapper_ultrasonic_sensor_hal.cpp.o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/fsjowbnuUltrasonic.cpp.o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/leduwjsmobjmodule.c.o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/fxqrvjwuparse.c.o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/hqaefmntqstr.c.o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/wahfyevd__init__.c.o -o /var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/Ardupy --specs=nano.specs --specs=nosys.specs -mcpu=cortex-m4 -mthumb -Wl,--cref -Wl,--check-sections -Wl,--gc-sections -Wl,--unresolved-symbols=report-all -Wl,--warn-common -Wl,--warn-section-align -Wl,--start-group -lm /Users/golden/.config/aip/ardupycore/ArduPy/lib/libarm_cortexM4lf_math.a -mfloat-abi=hard -mfpu=fpv4-sp-d16 -Wl,--end-group 
/var/folders/h3/bd3k3jr527vf6_4rdq9h4qw40000gn/T/tmpa51fm6ri/Ardupy  :
section              size        addr
.text              290392       16384
.ramfunc               32      306776
.ARM.exidx              8      306808
.data                 432   536870912
.hsram               1024   536871344
.bss               191056   536872368
.ARM.attributes        48           0
.comment              240           0
.debug_info       1600486           0
.debug_abbrev      138683           0
.debug_aranges      21520           0
.debug_ranges       30008           0
.debug_line        212713           0
.debug_str         163071           0
.debug_frame        70816           0
.debug_loc         309661           0
.stab                 204           0
.stabstr              441           0
Total             3030835


Firmware path: /Users/golden/.config/aip/deploy/Ardupy.bin
Usage:
    aip flash                                                                                                                                                                        /9.5s
➜  wio-terminal aip flash
Using cached http://files.seeedstudio.com/arduino/tools/x86_64-apple-darwin/bossac-1.8-48-gb176eee-i386-apple-darwin16.1.0.tar.gz (39 kB)
ERROR: Exception:
Traceback (most recent call last):
  File "/usr/local/lib/python3.7/site-packages/pip/_internal/cli/base_command.py", line 188, in _main
    status = self.run(options, args)
  File "/usr/local/lib/python3.7/site-packages/aip/flash.py", line 142, in run
    stty = self.stty
  File "/usr/local/lib/python3.7/site-packages/aip/flash.py", line 97, in stty
    return "stty -f " + self.port + " %d"
TypeError: can only concatenate str (not "NoneType") to str                                                                                                                          /1.1s
➜  wio-terminal aip board
ERROR: Sorry, the device you should have is not plugged in.                                                                                                                          /0.5s

Since then, it no longer connect via USB.

on a MAC, try this:

ls /dev/cu.*

Still nothing appears?

Normally it should be like this:

Screen Shot 2020-05-12 at 1.45.56 AM

I’m sorry that this happened. This may be caused by bootloader damage . Do you have a JLINK device? We will give you a tutorial on how to solve this problem.

I do not have a JLINK device. But, I’m sure I can get one.

Will this one work?
https://smile.amazon.com/Segger-J-Link-EDU-mini-Debugger/dp/B0758XRMTF/ref=sr_1_4?dchild=1&keywords=JLINK&qid=1589274776&sr=8-4

What is the best choice for JLINK device to Mac or Linux?

Do you have any other PC devices and do they also not recognize Wio Terminal?

Or does your device recognize other devices?

You can try a quick reset more than twice (for example, four times, six times), and then when you see that the blue LED starts to show the breathing light, it can work normally. Notice, it’s not flashing, it’s breathing

We’re trying to replicate what happened to you.

It works!!!

I used another Mac.

I noticed that the USB port goes up and down - until, I finally connected and flashed.

Seems to work fine, now! … I look forward to playing with it more!!

Thanks for your support!!!

Good to hear :smiley: