Hello,
since the default serial debug port for L4T is the UART2, I would like to use it on the A203v2 board (and not have to change the configuration files). The pinout only mentions the RX pin (14-pin connector W7, pin 10). Where is the TX pin?
Hello,
since the default serial debug port for L4T is the UART2, I would like to use it on the A203v2 board (and not have to change the configuration files). The pinout only mentions the RX pin (14-pin connector W7, pin 10). Where is the TX pin?
Hey @Frei_Herr, The pinout documentation is incorrect for the 14-pin (W7) Connector. Pin 9 is UART2_TX (not GND). Hope that helps!