UART WIFI V1.0 NEVER WORKED

Hello,



I acquired months ago an UART WIFI MODULE V1.0.

Despites hours of trial, I never manged to make it work on Ardunio, following the example given here :

http://wiki.seeedstudio.com/Grove-UART_Wifi/.



I acquired this week an UART WIFI MODULE V2.0.

I managed to make it working with your example, without any trouble, withing five minutes after unpacking it !



I suppose you changed more than you describe between V1.0 and V2.0 modules (firmware for AT commands ?).

Can you help me with my V1.0 module taking into account the facts that I demonstrated that I did no mistake in my trials ?



Best regards



Yannick

Hi Yannick



We suggest follow <LINK_TEXT text=" http://wiki.seeedstudio.com/Grove-UART … are-update"> http://wiki.seeedstudio.com/Grove-UART_Wifi/#firmware-update</LINK_TEXT> to do firmware update. then use AT command to test. <LINK_TEXT text=“http://wiki.seeedstudio.com/Grove-UART_ … t-commands”>http://wiki.seeedstudio.com/Grove-UART_Wifi/#at-commands</LINK_TEXT>. by the way, i have 2 wifi v1.0 on hand. One is without any return and the other works well. please let us know the result. thanks.



Bill

Hello Bill,

Thank you for your answer.

I’ll tell you the results as soon as possible !



Best regards



Yannick