Transparent transmission application

Hello

I defined Transparent transmission application in automatic working mode (cmd=AT+ATRM=0,0,192.168.1.100,1000) and saved values to flash, how can I exit from this mode

hello

you should use the escape sequence! I think it was AT+] and then you are in cmd mode again,

maybe to send a factory reset AT+RSTF

Its not working for me!!

Isn’t the escape sequence AT+& or 1B(in hex format) ?

When 1B is sent in hex format it enters the second boot mode. But i was not able to enter the at command mode ?