šŸ’„ The Xiao gets a Debugger... Seeedineers make MAGIC!

Hi there,

So I was able to get it going after a few cups of joe and this late night.
works with both GDB command line debug and with PlatformIO. The trick was NOT to use the OpenOcd builtin to PLIO. Once I set up the generic OpenOcd and the Device manager had the driver for the CMSIS-DAP device (interface 2) as none WinUSB.sys Zidag changed that and BAM! bob is your UNCLE debugger! :grin:
I’ll post a video in action but it’s fast , runs the 921600 baud, flashing is turbo quick.
here are the OpenOcd, GDB and PLIO snaps. target was a Xiao Nrf52840 Sense. Single stepping like a BOSS! :+1:


samd21 and Nrf52840 are verified!! so ESP32"s on deck…

HTH
GL :slight_smile: PJ :v:

If they can make this inexpensive everyone will want one. :crossed_fingers:

  • I can see User mode: press a ONE button , unbrick a Xiao. (restore the Bootloader)
  • I can see Maker mode: ā€œadvanced menuā€ add your own custom ,hex,bin, uf2 files.
  • I can see Developer mode: ANYTHING GOES!!! :smile:

Ok Seeedineers get Cooking! :v: