The Future of ESP Device Management is HERE (And It's Browser-Based!)

Say goodbye to juggling half a dozen desktop applications, command-line tools, and complex dependencies! ESPConnect is the revolutionary, zero-installation, browser-based control center for your ESP32 and ESP8266 boards. This single utility handles everything from file system management (SPIFFS/LittleFS), partition mapping, comprehensive flash backups, and firmware deployment, all without downloading a single piece of software. If you work with ESP chips, this tool will redefine your workflow.

• Device Awareness: Instant readout of chip family, MAC address, flash size, and capabilities.
• Storage Management: Full graphical mapping of partitions (Partitions Tab) for layout confirmation.
• File System Explorer: Seamless browsing, uploading, downloading, and formatting of SPIFFS, LittleFS, and FATFS.
• Maintenance & Backups: Easy flash firmware deployment, integrity checks (MD5), and full or partial chip backups.
• Live Monitoring: Integrated Serial Console for streaming logs and sending commands.
• OTA Slot Insights: View active and staged application slots with build metadata.

Hi there,

It’s a pretty great tool for beginners and makers, It can give/Show you some insight as to what’s inside and how it is configured.

Check it out, :+1: New users definitely will benefit from it.
Here is a screen of the S3
HTH
GL :santa_claus: PJ :v:

Another point it’s just a Browser Interface, BTW , you can Host a local version , Bare metal or Docker containers… I will try it locally it’s a great Idea , Nordic tried with there Visual Device tree but this is the best so far!. Arduino could learn from this. :v: