TFT Touch Shield V2.0 and Arduino Proto Shield

OK, then that is a problem. The version 1.0 shield uses a lot more of the digital pins passing information to the touch shield via an 8 bit parallel interface. I wqs not able to use it on my project at all as there were not pins available for my interface to the outside world and I also needed the SDCard to do datalogging and the version 1.0 touch shield and the SD shield had conflicts and would not work together. The version 2.0 shield with its built-in microSDcard was the answer.