T 1000 E Firmware Update not working

Yes. I’ve used it on other devices (RAK/T-Echo) and didn’t have an issue. Before I tried updating it, I was able to get this onto the mesh with my other nodes. My other nodes are running 2.5.15, so I wanted to update the T1000-E’s so all my nodes are on the same firmware. The T-1000’s were the first time I tried wiping the flash first, as they recommend. This is where I’m stuck. I’m suspecting that something happened with the erase and it won’t let a new firmware to be flashed properly.